Environmentally hazardous materials are defined as materials
that may be harmful to the human body or ecosystems
when contained in a product. In principle, we prohibit the
use of such materials in our components and raw materials.
For hazardous substances that may be present as impurities,
we have established tolerances and handle such
materials accordingly.
With regard to the Restriction of Hazardous Substances
Directive (RoHS)1 and REACH Regulation2 in the EU and
the Administrative Measure on the Control of Pollution
Caused by Electronic Information Products3 in China, we
have adopted our Green Procurement Guidelines at our
production facilities in and outside of Japan and provide
information necessary to meeting our customers’ requirements.
In addition, we submit REACH reports to the relevant
authorities as required.
We stringently manage chemicals specified in the PRTR
Law4 and are working to switch to products that do not
contain such substances. Our goal is to reduce our handling
of these chemicals by 3% each year, and we achieved
a reduction from last year, going from 37,962 kg in 2020 to
33,950 kg in 2021. Please visit our homepage for details
about our initiatives at each production facility.
| Substance | Amount | Air Emissions |
|---|---|---|
| Xylene | 1,308 | 191 |
| Toluene | 2,525 | 458 |
| Ethylbenzene | 375 | 60 |
| Benzene | 120 | 28 |
| Methylnapthalene | 26,166 | 55 |
| Other | 3,456 | 172 |
| Total | 33,950 | 963 |
The LM Guide washing process in Factory 1 used to employ Asahiklin AK-225, which contains dichloropentafluoropropane (also known as HCFC-225). Due to a change in the law, the manufacture of products containing this substance was banned in 2019. The remaining inventory was used in 2020, but in January 2021, the plant switched to products not made with HCFC-225, thereby reducing the handling of that chemical by 575 kg per year.