General industrial machinery
![Automatic Packing Machine for Foodstuffs/Medicine](/sites/default/files/thkcom/images/ja/products/industry/general_industrial.png)
Various types of manufacturing machines are being used for automation and labor saving purposes in fields where production was previously carried out by manual labor. THK's products are being used in this context, from devices which simply repeat the same operation accurately and efficiently to those enabling craftsperson-like precision.
Electric injection molding machines
From hydraulic energy requiring electricity. Environmental concerns have led many manufacturers to move to injection-molding machines driven by electric power. In these machines, heavy load-type Ball Screws with the same tightening force as conventional hydraulic cylinders are used, along with highly rigid LM Guides for accurate die positioning.
Punching presses
How quickly can you punch through? Punching speeds are continually accelerating, and Ball Screws with a large lead are ideal for moving thin steel plate workpieces with high acceleration or deceleration. To allow for such high-speed work movement, Caged Ball LM Guides and Ball Screws are used.
Resin welding equipment
To weld two resin tubes, they must be simultaneously heated and pushed together along a straight line with a fixed pressure. This accurate and reliable soldering quality can be ensured by positioning those tubes with LM Guides.
Horizontal compression baling machines
Caged Ball LM Guides and Precision, Caged Ball Screw Model HBN are used in the electric drive systems of scrap paper compression baling machines in paper factories. In the past, hydraulic cylinders were used to move compression press formworks, but oil leaked and deteriorated during equipment maintenance, contaminating both the refuse paper and the equipment peripherals. However, by moving to a motor drive system in conjunction with Ball Screw Model HBN, which exhibit resistance to high load equal to hydraulic cylinders, the oil leakage problem was eliminated. What's more, this also allowed the baling machines to be made more compact.
Products used
LM Guide (Linear Motion Guide)
The LM Guide (Linear Motion Guide) is our main product, which incorporates a component with a linear rolling motion into practical use for the first time in the world.
Ball Screw
The Ball Screw is a high-efficiency feed screw with the ball making a rolling motion between the screw axis and the nut.
Ball Spline
The Ball Spline is a rolling guide spline bearing.
LM Guide Actuator
The LM Guide Actuator is a compact actuator with high rigidity and high precision that has an integrated LM Guide with a ball screw.
Slide Pack
The Slide Pack is an inexpensive linear guide configured with the press-formed slider and roll-formed rails.
Slide Rail
The Slide Rail is a low-priced limited-type linear guide made of steel plate precision-formed by rolling.
Linear Bushing
The Linear Bush is a linear guide used in combination with a LM shaft that has a cylindrical shaft.
Change Nut
The Change Nut is a sliding feed screw of 45° lead angle not easily available from machining.
Cam Follower
The Cam Follower is a compact bearing with a high-rigidity shaft and a built-in needle bearing.
Lubrication accessories
An assortment of lubrication associated products is available to maintain sufficient lubrication of machines.